cancel
Showing results for 
Search instead for 
Did you mean: 

Linker offsets for bootloader -> IRQs do not work any more

HMüll.4
Senior

Hi,

I have some CubeMX-generated code which works properly. Originally it was created to run from default address 0x08000000.
Now I have a bootloader at address 0x08000000 which is responsible for handling updates and other stuff and then jumps into the target-code, so I moved that code via linker script to 0x08020000. This also works fine, the code works as desired.
In a next step I decided to have some additional information stored in flash prior to the CubeMX generated code to make it easier for the bootloader to manage firmware versions, so I shifted the code by additional 128 bytes and now have the following section in my linker script:

MEMORY
{
  FLASH_BOOT (rx)   : ORIGIN = 0x08000000, LENGTH = 128K
  FLASH (rx)        : ORIGIN = 0x08020080, LENGTH = 1024K - 128K - 128
  EEPROM_EMUL (xrw) : ORIGIN = 0x080E0000, LENGTH = 128K
  DTCMRAM (xrw)     : ORIGIN = 0x20000000, LENGTH = 128K
  RAM_D1_DMA (xrw)  : ORIGIN = 0x24000000, LENGTH = 64K
  RAM_D1 (xrw)      : ORIGIN = 0x24010000, LENGTH = 320K - LENGTH(RAM_D1_DMA)
  RAM_D2 (xrw)      : ORIGIN = 0x30000000, LENGTH = 32K
  RAM_D3 (xrw)      : ORIGIN = 0x38000000, LENGTH = 16K
  ITCMRAM (xrw)     : ORIGIN = 0x00000000, LENGTH = 64K
}

My problem: with the start offset of 0x08020080 my interrupts do not work any more. So what is the problem here? What do I have to do in order to work with an application offset different than 128K?

Thanks!

 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

The offset needs to be a multiple of 0x400 on the H7, as @waclawek.jan suggests.

https://community.st.com/t5/stm32-mcus-products/multiple-value-for-vect-tab-offset-on-stm32h7/td-p/613292

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

5 REPLIES 5
waclawek.jan
Super User

Do you set SCB_VTOR to reflect this?

JW

This seems to be already covered by the changes in the linker script. On initialisation, in SystemInit(), within the statement

SCB->VTOR = (uint32_t) g_pfnVectors;

 

that g_pfnVectors points to the changed address 0x08020080

 

waclawek.jan
Super User

Which STM32?

If the vector table is longer than 0x80 - which probably in all 'H7 is - you can't have it at 0xXXXXXX80 address.

JW

Vidar
Associate III

Can you maybe share more information about the MCU you use?

Do you really have a 1MB internal flash? I would think you have a H7, but share more info to be sure

TDK
Super User

The offset needs to be a multiple of 0x400 on the H7, as @waclawek.jan suggests.

https://community.st.com/t5/stm32-mcus-products/multiple-value-for-vect-tab-offset-on-stm32h7/td-p/613292

If you feel a post has answered your question, please click "Accept as Solution".