2026-05-13 5:54 AM
Hello,
I noticed that when showing differences between the current and the previous generated source code the width of the source code window does not even show 80 characters even though there is plenty of room in the application window (see screenshot attached). I spent quite a bit of time looking at the HAL source code when debugging and the source code is not formatted to 80 character lines anyway. Sometimes it exceeds 80 by a wide margin.
Would it make sense to show the source code window as a popup or as wide as the application window allows?
Thank you,
Gil
2026-05-13 6:50 AM
Hi @gil_dobjanschi ,
Thank you for the feedback and for sharing the screenshot.
We understand the issue you are seeing with the source code preview width, especially when comparing generated code and reviewing HAL source files that exceed 80 characters per line.
We do have two internal tickets currently tracking possible improvements in this area:
These items are currently under feasibility review, and I will keep you posted on any decision or planning.
Internal ticket number: CDM0062617 and CDM0062618 (This is an internal tracking number and is not accessible or usable by customers).
Regards,
Sara.
2026-05-13 7:02 AM
Thank you @Sara BEN HADJ YAHYA !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.