Possible Bug in cubeMX 5.6.1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-17 2:15 AM
Not really an issue, but it is worth mentioning...
inside cubeIDE, i generate a new stm32 project, in target selector i select the nucleo f446re board and initialize it with the standard peripheral settings. When checking the clock configuration, i would expect the HCLK at 180MHz (which is max for that mcu). Unfortunately it´s set to 84MHz, like a f401. It´s no problem to enter just 180 there and let the "Resolve Clock Issues"-Button do the job here, but anyway: it´s a little bit strange ...
Edit: This applies to both versions. cubeMX stand alone and the integrated one in cubeIDE
- Labels:
-
STM32CubeMX
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-29 9:48 PM
Hello @Karl Hönemann
Thanks for the feedback,
Temporarily you have to configure the board manually.
Best regards,
Nesrine