2024-05-09 04:36 PM
Somewhere between CubeMX 6.9 and 6.11 a bug has been introduced that reports the PLLQ can only be less than 33MHz.
It is not honouring the Voltage scale set in the RCC parameters.
I have set the voltage scale to "Scale 1" but it still reports the PLLQ to be limited to 32MHz which is actually "Scale 2"
Solved! Go to Solution.
2024-05-09 11:30 PM - edited 2024-05-09 11:46 PM
Hello @euanbrown and welcome to the ST Community 😊.
Thank you for reporting this issue. I've been able to reproduce this issue and I've reported to the concerned team for correction (under internal ticket number 181096).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-09 11:30 PM - edited 2024-05-09 11:46 PM
Hello @euanbrown and welcome to the ST Community 😊.
Thank you for reporting this issue. I've been able to reproduce this issue and I've reported to the concerned team for correction (under internal ticket number 181096).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.