2020-09-08 5:18 AM
Hello,
I have found a difference between the PLL input frequency specification between the datasheet of the L4S5 :
And CUBEMX data :
Datasheet limit is at 16MHz, CUBEMX limit is at 8MHz.
Is there any errata sheet tht specify this difference?
Thank you for your answer,
Sincerely,
Guillaume
2020-09-08 11:11 AM
Hello @GChat.1 ,
I will forward this issue internally to check, then will come back to you with update.
Best Regards,
Imen
2020-09-11 8:52 AM
Hello @GChat.1 ,
After check, according to the datasheet :
"- 4 to 48 MHz high-speed external crystal or ceramic resonator (HSE), that can supply a PLL.
The HSE can also be configured in bypass mode for an external clock.
- 16 MHz high-speed internal RC oscillator (HSI16), trimmable by software, that can supply a PLL
...
"
The PLL input frequency can be used :
and it's the case using CubeMX.
The Default value in the Clock config Panel - Input Frequency is 8MHz, but it can reach 48MHz (you need just to enable the RCC HSE).
Best Regards,
Imen
2020-09-11 9:20 AM
Certainly in prior designs the HSI was a pulse generator, so not 50/50 duty, and thus needed a flip-flop to divide by 2 and give a clean 50/50 clock source.
The PLL's VCO is very much a rapid pulse generator, again the reason the PLL clocks needing a DIV2, DIV4, etc on the output as the core needs a 50/50 clock as it uses both phases.
2020-09-11 9:55 AM
Thank you for your feedback,
My question is more simple :
Why CUBEMX returns an error when I set a PLL input frequency greater than 8MHz as the input limit indicated in the datasheet page 165 is :
" fpll_in min : 2,0645 MHz ; fpll_in max : 16MHz"
Thank you for your new feedback,
Sincerely,
Guillaume