cancel
Showing results for 
Search instead for 
Did you mean: 

PIN NO.F1 of H750XBH6 in its datasheet differs from stm32cubemx

Tokit
Associate II

Tokit_0-1708613819435.png

Tokit_1-1708613829460.png

In datasheet it's NC while stm32cubemx says it's VSS

It doesn't matter I think

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Tokit 

As you can see here:

STTwo32_0-1708614675193.png

The PIN NO.F1 is compatible on datasheet (DS12556Rev7) and CubeMX configuration. I think you are using an old revision that has been updated.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
STTwo-32
ST Employee

Hello @Tokit 

As you can see here:

STTwo32_0-1708614675193.png

The PIN NO.F1 is compatible on datasheet (DS12556Rev7) and CubeMX configuration. I think you are using an old revision that has been updated.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Peter BENSCH
ST Employee

@Tokit some additional information: the data sheet from which you took the screenshot is the old rev 6. The screenshot from @STTwo-32 is from the newer and corrected rev 7.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks.Datasheet on semiee is outdated