cancel
Showing results for 
Search instead for 
Did you mean: 

PA0_C GPIO PIN

BAl K.1
Associate III

I have stm32h745i-disco for my project and use PA0_C and PC_3 for output. and when i use usual HAL_GPIO_WritePin() it is not working. Should i change something to make it work? Please help

 

1 ACCEPTED SOLUTION

Accepted Solutions
Sarra.S
ST Employee

Hello @BAl K.1, thank you for your post, 

Make sure you configured the GPIO pins, enabled GPIOA, GPIOC

Your code should look something like this : 

/* Enable GPIOA and GPIOC clock */ __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); /* Configure PA0 and PC3 as outputs */ GPIO_InitTypeDef GPIO_InitStruct = {0}; GPIO_InitStruct.Pin = GPIO_PIN_0; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_3; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); /* Set the output value of PA0 and PC3 */ HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET); HAL_GPIO_WritePin(GPIOC, GPIO_PIN_3, GPIO_PIN_RESET);

Hope that helps!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Sarra.S
ST Employee

Hello @BAl K.1, thank you for your post, 

Make sure you configured the GPIO pins, enabled GPIOA, GPIOC

Your code should look something like this : 

/* Enable GPIOA and GPIOC clock */ __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); /* Configure PA0 and PC3 as outputs */ GPIO_InitTypeDef GPIO_InitStruct = {0}; GPIO_InitStruct.Pin = GPIO_PIN_0; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_3; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); /* Set the output value of PA0 and PC3 */ HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET); HAL_GPIO_WritePin(GPIOC, GPIO_PIN_3, GPIO_PIN_RESET);

Hope that helps!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you, it works