2021-05-16 03:32 AM
I have created a project as in the video (https://www.youtube.com/watch?v=PalTKoMf_Xo&t=276s), however in my case there is an extra tab as "Platform Settings" in Middlewares->LWIP and it gives warning. After that, I couldn't take an IP address from my modem. I used DHCP.
Is this normal? Should I leave as it default or should I choose LAN8742 as a solution
2021-05-16 07:31 AM
Do you use USB as network device (modem)?
The LAN... is Ethernet PHY, in this case you can ignore it (let the Cube do whatever it wants, then remove unneeded stuff).
--pa