cancel
Showing results for 
Search instead for 
Did you mean: 

No SPI DMA example for nucleo-h563zi board in CubeMX

WCarey
Associate III

WCarey_0-1712029578460.png

Hi,

I am unable to find a SPI_FullDuplex_ComDMA_Master/Slave examples for the NUCLEO-H563ZI board in CubeMX (v6.11.0). Can you please point where this example can be found?

Thanks in advance

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STTwo-32
ST Employee

Hello @WCarey 

For the NUCLEO-H563ZI we only have SPI_FullDuplex_ComPolling_Master/Slave and SPI_FullDuplex_ComIT_Master/Slave examples. If you are looking for the SPI_FullDuplex_ComDMA_Master/Slave, you can refer to the examples based on the NUCLEO-H503RB. And try to adapt them to the NUCLEO-H563ZI.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.