2024-12-30 6:24 AM
I want to synchronize two SAI interfaces together, but I can not select the "Synchrounous slave" option unless I enable master block in the same SAI. I Have Master enabled in the other SAI and "External Synchro out" as well. When I enable Master in the same SAI, I can even select other SAI as the Sync input. It seems like a bug, but maybe I'm missing something. Im using CubeMX 6.12.0 and STM32H563ZIT6. Thanks
Solved! Go to Solution.
2025-01-03 5:04 AM - edited 2025-03-05 7:12 AM
Hello @matyasreznicek
This has been escalated internally (under internal ticket number 199546). I will be back to you as soon as I have a feedback.
PS: Issue solved on the last release of the STM32CubeMX
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-30 7:29 AM
Hello @matyasreznicek @and welcome to the ST Community.
First, i suggest you try using the last version of the STM32CubeMX V6.13.0. If you still have a problem, please add your .ioc file in a comment.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-30 4:20 PM
2025-01-03 5:04 AM - edited 2025-03-05 7:12 AM
Hello @matyasreznicek
This has been escalated internally (under internal ticket number 199546). I will be back to you as soon as I have a feedback.
PS: Issue solved on the last release of the STM32CubeMX
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.