cancel
Showing results for 
Search instead for 
Did you mean: 

Login problem

ofsong
Associate

屏幕截图 2024-09-05 172733.png

4 REPLIES 4
mƎALLEm
ST Employee

Hello @ofsong and welcome to the community.

Do you have a proxy? if yes indeed you need to configure it in Help -> "Updater Settings" -> "Connection parameters"

Otherwise you can set it to "No Proxy"

SofLit_0-1725528849225.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
STTwo-32
ST Employee

Hello @ofsong 

You can also refer to this article to understand how this works.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

对我设置的无代理,然后登录一直显示这个屏幕截图 2024-09-05 174534.png屏幕截图 2024-09-05 174627.png

Try to restart CubeMX. If you are not using the last version, please update to your tool. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.