2020-06-09 10:27 AM
CubeIDE 1.2.0
I have a simple script to test the command line setup. The script is loading the .ioc and creating .csv of the pinout.
I get partially through the csv command where Java runs into a NullPointerException seen below
2020-06-09 12:53:23,629 [DEBUG] PinoutAndConfigurationView:553 - sp_PinoutAndSystemViews - pce.getPropertyName() : dividerLocation1.0
2020-06-09 12:53:23,629 [DEBUG] PinoutAndConfigurationView:691 - sp_ModeConfig - pce.getPropertyName() : dividerLocation0.5
2020-06-09 12:53:23,649 [DEBUG] PinoutAndConfigurationView:960 - Start propertyChange PinoutAndConfigurationView : preferredSize
2020-06-09 12:53:23,649 [DEBUG] PinoutAndConfigurationView:1030 - End propertyChange PinoutAndConfigurationView : preferredSize
2020-06-09 12:53:23,649 [DEBUG] PinOutPanel:732 - fitInWindow Computed Zoom: 0.5
2020-06-09 12:53:23,692 [DEBUG] PinOutPanel:732 - fitInWindow Computed Zoom: 0.5
2020-06-09 12:53:23,754 [DEBUG] PinoutAndConfigurationView:1447 - Resize component
2020-06-09 12:53:23,754 [DEBUG] PinOutPanel:732 - fitInWindow Computed Zoom: 0.5
java.lang.NullPointerException
at com.st.microxplorer.mcu.Mcu$37.onCommandEntered(Mcu.java:3641)
at com.st.components.util.CommandLineManager.onCommandEntered(CommandLineManager.java:155)
at com.st.components.util.CommandLineManager.runCommand(CommandLineManager.java:172)
at com.st.components.util.CommandLineManager.runCommand(CommandLineManager.java:188)
at com.st.components.util.CommandLineManager.runCommand(CommandLineManager.java:331)
at com.st.components.util.CommandLineManager.onCommandEntered(CommandLineManager.java:414)
at com.st.components.util.CommandLineManager.onCommandEntered(CommandLineManager.java:140)
at com.st.components.util.CommandLineManager.runCommand(CommandLineManager.java:174)
at com.st.components.util.CommandLineManager.runCommand(CommandLineManager.java:331)
at com.st.microxplorer.maingui.MicroXplorer.run(MicroXplorer.java:246)
at com.st.microxplorer.maingui.STM32CubeMX.run(STM32CubeMX.java:25)
at com.st.microxplorer.maingui.STM32CubeMX.main(STM32CubeMX.java:40)
KOHow do I download or add the offending components? I am not sure exactly how to fix this issue.
2020-06-09 1:19 PM
Not sure you're going to get much support with v1.2.0. Updating to v1.3.1 might yield different results.
2020-06-09 1:40 PM
Ok then reply as if I was on 1.3.1 ...
I am in CubeIDE version 1.2, which is using Cube MX version 5.6.1 which is the latest version of CubeMX. And since this is a CubeMX command the IDE version should not matter now that I think of it.
Also referencing Document UM1718 V31 December 2019 section 3.3.2 for command line and scripting commands
Detected Java Version = 1.8.0_202