Skip to main content
Associate III
Dec 10, 2025 9:11 AM UTC
Question

"Cannot connect to access port 0!" error while programming STM32U575VIT6Q

Hello everyone,

I’m currently facing a blocking issue with SWD programming on an STM32U575VIT6Q placed on a custom PCB.
Until today everything worked correctly: I use a CLI-based flashing procedure that programs a set of binary files (around a dozen) using commands like the following:

%CLI_EXEC% -vb %VERBOSITY% -c port=swd dLPM -w "filename" %address% -v

The entire flashing sequence has always completed successfully, but during the last programming cycle I suddenly received the following error:

Error: Cannot connect to access port 0!
If you are trying to connect to a device with TrustZone enabled please try to connect with HotPlug mode.
If you are trying to connect to H5 device and your target is already locked with password or certificate, please open your device using Debug Authentication.

Since that moment, I have been completely unable to connect to the MCU with my ST-Link V2 in any mode.
I tried:

  • Normal

  • Under Reset

  • Hot Plug

  • Power-down

Unfortunately, all attempts fail with the same error.

A few details that may help:

  • TrustZone was never enabled on this device.

  • I never configured PCROP or any type of Flash/OB protection.

  • The same programming script works flawlessly on an STM32U585 placed on another custom PCB (pretty much similar to the current one).

  • STM32CubeProgrammer v2.19.0

At this point the device seems completely inaccessible over SWD.
Has anyone experienced similar behavior, or can suggest how to recover the MCU?
What would be the recommended procedure when Debug Authentication is mentioned even though no protection was intentionally set?

Any help would be greatly appreciated.

Thanks in advance.

 

2 replies

pa0grgAuthor
Associate III
Dec 15, 2025 4:09 PM UTC

Anyone? May this problem be ESD related?

pa0grgAuthor
Associate III
Dec 16, 2025 3:59 PM UTC

Hello, 

since this has been a really huge issue for me, I wanted to publish "Cannot connect to access port 0!" error while programming STM32U575VIT6Q issue in this section too since in the past was really helpful.

 

Logs:
ST-LINK SN : 36FF72065648343836081143
ST-LINK FW : V2J46S7
Board : --
Voltage : 3.21V
Error: Unable to get core ID
Error: Cannot connect to access port 0! If you are trying to connect to a device with TrustZone enabled please try to connect with HotPlug mode. If you are trying to connect to a device which supports Debug Authentication with certificate or password, please open your device using it.

I really don't know what to do, the application flashed at 0x08000000 seems to start but I can't connect through SWD in any possibile way. I've tried anything, even Hot Plug mode as suggested bt STM32CubeProgrammer (latest release).

The only HAL function which I think could cause some trouble might be:

HAL_DBGMCU_DisableDBGStopMode();

 

Thanks in advance.