cancel
Showing results for 
Search instead for 
Did you mean: 

It's 3 times slower - my one microsecond timer configured by CubeMX running on NUCLEO-C031C6 (STM32C031C6)

RongShengWang
Associate III

Hi, 

     My one microsecond timer configured by CubeMx running on NUCLEO-C031C6 (STM32C031C6) is 3 times slower than it should be. The code is attached below.

      the call "delay_us(60000000);" takes 3+ minutes to complete - it should be done in one minute.

      The LL timer (TIM3) init and interrupt code is generated by CubeMx..The system clock is 48 MHZ in CubeMx.

       How to fix it?

       Thanks,

      Rong

 

 

 

void MX_TIM3_Init(void)
{

  LL_TIM_InitTypeDef TIM_InitStruct = {0};

  /* Peripheral clock enable */
  LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_TIM3);

  /* TIM3 interrupt Init */
  NVIC_SetPriority(TIM3_IRQn, 0);
  NVIC_EnableIRQ(TIM3_IRQn);

  /* USER CODE BEGIN TIM3_Init 1 */

  /* USER CODE END TIM3_Init 1 */
  TIM_InitStruct.Prescaler = 0;
  TIM_InitStruct.CounterMode = LL_TIM_COUNTERMODE_UP;
  TIM_InitStruct.Autoreload = 48;
  TIM_InitStruct.ClockDivision = LL_TIM_CLOCKDIVISION_DIV1;
  LL_TIM_Init(TIM3, &TIM_InitStruct);
  LL_TIM_EnableARRPreload(TIM3);
  LL_TIM_SetClockSource(TIM3, LL_TIM_CLOCKSOURCE_INTERNAL);
  LL_TIM_SetTriggerOutput(TIM3, LL_TIM_TRGO_RESET);
  LL_TIM_DisableMasterSlaveMode(TIM3);
  /* TIM3 interrupt Init */
}

/* USER CODE BEGIN 1 */
unsigned long u_Count = 0;
/* USER CODE END 1 */
/**
  * @brief This function handles TIM3 global interrupt.
  */
void TIM3_IRQHandler(void)
{
  /* USER CODE BEGIN TIM3_IRQn 0 */

  if (u_Count)
  {
	  u_Count--;
  }
  if (LL_TIM_IsActiveFlag_UPDATE(TIM3))
 	LL_TIM_ClearFlag_UPDATE(TIM3);
  /* USER CODE END TIM3_IRQn 0 */
}

void delay_us(const unsigned long us_Count)
{
	u_Count = us_Count;
	LL_TIM_EnableIT_UPDATE(TIM3);
	LL_TIM_EnableCounter(TIM3);
	while (u_Count !=0) 
        {
        }
	LL_TIM_DisableIT_UPDATE(TIM3);
	LL_TIM_DisableCounter(TIM3);
}

int main(void)
{
  static unsigned int i = 0;
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* Configure the system clock */
  SystemClock_Config();

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_TIM3_Init();
  MX_SPI1_Init();
  MX_USART2_UART_Init();

  delay_us(60000000);
}

 

 

   

1 ACCEPTED SOLUTION

Accepted Solutions

Perhaps you could review examples?

STM32Cube_FW_C0_V1.0.1\Projects\NUCLEO-C031C6\Examples_LL\TIM\TIM_TimeBase_Init

 

/* Enable counter */
LL_TIM_EnableCounter(TIM3);

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

11 REPLIES 11
TDK
Guru

The chip cannot process interrupts at 1 MHz. It will fall behind. Set your interrupt frequency to a max of about 10 kHz so one interrupt can finish before the next one is triggered.

Also note that if you have a timer frequency of 48 MHz, you want ARR=47 in order to have an update interval of 1 us. So for 10 kHz, it should be 4799.

If you feel a post has answered your question, please click "Accept as Solution".

As repeatedly covered on this forum, you can't sustain 1 MHz interrupt rate, it will saturated the processor just trying to do that. So don't do it that way.

Configure the TIM in maximal mode, say 0xFFFF or 0xFFFFFFFF with a prescaler that clocks the count at 1 MHz, and then delta the entry and exit points.

uint16_t start =TIM3->CNT;

while((TIM3->CNT - start) < usdelay);

For finer resolution clock faster. For longer delays with 16-bit counters, decompose into 60 ms (60000 us) intervals

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi, Guru,

    So I can not have a 1 us timer, which I need,in STM32C031C6?, 

    What is the fastest timer I can have in this micro ?

Thanks

Rong

Hi, Tesla,

     Could you give me the detail code for having 1 us timers? 

     I used CubeMx to generate the code. 

     "Configure the TIM in maximal mode," - How to do this?

    Thanks,

 

Rong

 

 

void MX_TIM3_Init(void)
{

  /* USER CODE BEGIN TIM3_Init 0 */

  /* USER CODE END TIM3_Init 0 */

  LL_TIM_InitTypeDef TIM_InitStruct = {0};

  /* Peripheral clock enable */
  LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_TIM3);

  /* TIM3 interrupt Init */
  NVIC_SetPriority(TIM3_IRQn, 0);
  NVIC_EnableIRQ(TIM3_IRQn);

  /* USER CODE BEGIN TIM3_Init 1 */

  /* USER CODE END TIM3_Init 1 */
  TIM_InitStruct.Prescaler = 0;
  TIM_InitStruct.CounterMode = LL_TIM_COUNTERMODE_UP;
  TIM_InitStruct.Autoreload = 48;
  TIM_InitStruct.ClockDivision = LL_TIM_CLOCKDIVISION_DIV1;
  LL_TIM_Init(TIM3, &TIM_InitStruct);
  LL_TIM_EnableARRPreload(TIM3);
  LL_TIM_SetClockSource(TIM3, LL_TIM_CLOCKSOURCE_INTERNAL);
  LL_TIM_SetTriggerOutput(TIM3, LL_TIM_TRGO_RESET);
  LL_TIM_DisableMasterSlaveMode(TIM3);
  /* USER CODE BEGIN TIM3_Init 2 */
  /* TIM3 interrupt Init */

  /* USER CODE END TIM3_Init 2 */

}

 

 

Not using interrupts

 

  TIM_InitStruct.Prescaler = 48 - 1; // Divider 48 MHz to 1 MHz (1 us ticks)
  TIM_InitStruct.CounterMode = LL_TIM_COUNTERMODE_UP;
  TIM_InitStruct.Autoreload = 0xFFFF; // Maximal Count 0..65535
  TIM_InitStruct.ClockDivision = LL_TIM_CLOCKDIVISION_DIV1;

You're using it to count elapsed time, up to 65.535 ms per update period

 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
BarryWhit
Senior III

[withdrawn]

- If a post has answered your question, please acknowledge the help you received by clicking "Accept as Solution".
- Once you've solved your issue, please consider posting a summary of any additional details you've learned. Your new knowledge may help others in the future.

Hi, Tesla,

     Understand. I will try.

     Thank you very much. 

Rong

Hi, Tesla,

    The execution stucks in while((TIM3->CNT - start) < us_Count);

    Because TIM3->CNT does not increase. 

   I follow your email to have the initialization below. 

   Looks like need to add some API call to start running the counter?

   Please help, thanks,

  TIM_InitStruct.Prescaler = 48-1;
  TIM_InitStruct.CounterMode = LL_TIM_COUNTERMODE_UP;
  TIM_InitStruct.Autoreload = 0xFFFF;
  TIM_InitStruct.ClockDivision = LL_TIM_CLOCKDIVISION_DIV1;
  LL_TIM_Init(TIM3, &TIM_InitStruct);
  LL_TIM_EnableARRPreload(TIM3);
  LL_TIM_SetClockSource(TIM3, LL_TIM_CLOCKSOURCE_INTERNAL);
  LL_TIM_SetTriggerOutput(TIM3, LL_TIM_TRGO_RESET);
  LL_TIM_DisableMasterSlaveMode(TIM3);

 

Hi, Tesla,

    (Continue) - Looks like need to add some API call to start running the counter?

    HAL has "HAL_TIM_Base_Start() ". 

    What is the function for LL?

   Please help, thanks,

Rong