2018-12-26 4:28 PM
I do have a pretty decent computer. XEON 12 Core and 64GB RAM running Mac OS 10.14. But using this ST application is a terrible exercise in patience. Sometimes I need to double click things (e.g. TIMx under Timers on the left) so it changes to its settings. Over all version 5.0 is a real pain to use.
BUT maybe there is something "sub optimal" on my system. Especially Java. Are there other users that suffer from slow user interface with that application? What is the preferred Java version?
2018-12-26 9:49 PM
Looks like it's the same for everybody. If CubeMX laggs on a 4core i5 like in my case, then there is something bad.. Not even on 12 Core Xenon..