2017-04-19 05:42 AM
Hi All,
How can I install a new firmware package to stm32CubeMX. I tried to install
X-NUCLEO-IDW01M1 which is a wifi driver firmware package.
I downloaded the file (en.x-cube-wifi1_firmware.zip) and I tried to install it from cubemx, but I got an error:
'this package version is not managed on this version of STM32CubeMX'
I use Debian Linux, and my cubemx version is: 4.20.1 STM32Cube V1.0 on help/about
The zip file is not corrupted, I can unzip it and it has a directory:
STM32CubeExpansion_WIFI1_V3.0.1 and the directory contains a package.xml file:
<?xml version='1.0' encoding='ISO-8859-1' standalone='no'?>
<Package DBVersion='2.0'> <PackDescription Release='FW.WIFI1.3.0.1'> <Note Release='ReleaseNotes.html'/> </PackDescription></Package>thx
Zamek
#cubemx #firmware #local-install2017-04-19 05:55 AM
Hi,
The expansion package are not downloadable under STM32CubeMx. You should download the X-CUBE-WIFI1 package from ST web through this link
.Only Cube firmware package can be downloaded from this tool.
Thanks
Imen
2017-04-19 06:39 AM
Hi,
I belived that, I can use the expansions under cubemx.
ok, thx
2017-04-19 09:48 AM
Yes it is definitely a bit nonsensical..
The LoRaWAN stuff is free standing, really doesn't need/use Cube, but has it in the name, just uses the HAL libraries, and compiles as unpacked in Keil, IAR, etc.
2017-05-01 01:06 AM
Hi Zamek..
I'm also try configure the Ethernet in STM32f429 nucleo board , please share me your example code .
It's help full for me....I try to configure the Ethernet With respect to your example...
Best of regards
krishna