cancel
Showing results for 
Search instead for 
Did you mean: 

initialize all peripherals with their default mode not working reliably

ASmit.13
Associate

Is there any way to force the reset to defaults when the dialogue box does not come up asking you?

Using 1.6.1 of the stm32cubeide with L432 nucleo32 development board.

I have seen this once in a while but thought it was fixed in the latest version but a student in my class says it never asks him. So wondered if there is a workaround?

1 ACCEPTED SOLUTION

Accepted Solutions
Houda GHABRI
ST Employee

Hi @ASmit.13​ ,

If we start a project from Board we will necessarily have a pop up to ask user if he wants to initialize or not Ip with their default mode.

As mentioned by @TDK probably they are starting the project from MCU.

For your information, If we have a project already configured and you wants to reset modes there is an option in CubeMX from Pinout TAB to do it :

0693W00000Bb7oGQAR.pngHope this helps you.

If your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Houda

View solution in original post

2 REPLIES 2
TDK
Guru

Probably they are starting the project by selecting a chip and not the board.

If you feel a post has answered your question, please click "Accept as Solution".
Houda GHABRI
ST Employee

Hi @ASmit.13​ ,

If we start a project from Board we will necessarily have a pop up to ask user if he wants to initialize or not Ip with their default mode.

As mentioned by @TDK probably they are starting the project from MCU.

For your information, If we have a project already configured and you wants to reset modes there is an option in CubeMX from Pinout TAB to do it :

0693W00000Bb7oGQAR.pngHope this helps you.

If your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Houda