I would like to automate the CubeMX build. This is to support continuous integration via Jenkins. So far, cannot find the answers I'm looking for.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-21 3:49 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-22 2:23 AM
Hi @Community member,​
AFAIK CubeMX offer a CLI
refer to STM32CubeMX for STM32 configuration and initialization C code generation - User manual
Section
3.3.2 Running STM32CubeMX in command-line mode
Post redirect to STM32CubeMX topic for further support if needed
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-22 3:51 PM
Olivier,
Below is the batch file I am invoking from Jenkins to automate the CubeMX build. Following that is the CubeMX script file. When I run the batch file from the command file it works fine. Although I do get a progress bar during the "project generate" phase. Because I use the -q qualifier, I would not expect this progress bar. But when running from Jenkins I get the following:
Everything seems to be working fine until "project generate". I terminate after a few minutes. Could it be that CubeMX is trying to display the progress bar?
Batch file:
java -jar "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\STM32CubeMX.exe" -q "C:\JenkinsBuilds\workspace\ICELL8_Firmware\ICELL8_FirmwareScript.txt"
"C:\Program Files\IAR Systems\Embedded Workbench 9.0\common\bin\iarBuild.exe" "C:\JenkinsBuilds\workspace\ICELL8_Firmware\EWARM\ICELL8_Firmware.ewp" -make "Release" -log info
Script file:
config load "C:\JenkinsBuilds\workspace\ICELL8_Firmware\ICELL8_Firmware.ioc"
project generate ./
exit
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-01-05 10:39 AM
Olivier,
Below is the batch file I am invoking from Jenkins to automate the CubeMX build. Following that is the CubeMX script file. When I run the batch file from the command file it works fine. Although I do get a progress bar during the "project generate" phase. Because I use the -q qualifier, I would not expect this progress bar. But when running from Jenkins I get the following:
Everything seems to be working fine until "project generate". I terminate after a few minutes. Could it be that CubeMX is trying to display the progress bar?
Batch file:
java -jar "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\STM32CubeMX.exe" -q "C:\JenkinsBuilds\workspace\ICELL8_Firmware\ICELL8_FirmwareScript.txt"
"C:\Program Files\IAR Systems\Embedded Workbench 9.0\common\bin\iarBuild.exe" "C:\JenkinsBuilds\workspace\ICELL8_Firmware\EWARM\ICELL8_Firmware.ewp" -make "Release" -log info
Script file:
config load "C:\JenkinsBuilds\workspace\ICELL8_Firmware\ICELL8_Firmware.ioc"
project generate ./
exit