cancel
Showing results for 
Search instead for 
Did you mean: 

How to recover from FR_DISK_ERR during f_write in STM32

SSin
Associate III

Hi all,

I am now using SYM32F103RE to read data from codec via I2S & write into SD card. I use the HAL library in STM32CubeMX w/ Chen's fatfs & I2S DMA. Unlucky, f_write will sometime return FR_DISK_ERR. According to fatfs, I can only f_close the file in this case. But it only return FR_INVAILD_OBJECT no matter what I do. If I add a 1ms polling delay (HAL_Delay(1)) between each f_write, it works fine. So is there any way to avoid or recover from the problem?

Here is my code:

FRESULT u8_sd_fat_status = FR_DISK_ERR;   // 0 = SD card FAT file system is ok, otherwise 1.
uint16_t u32_array_codec_in[512];
 
f_mount(&SDFatFS, (TCHAR const*)SDPath, 0);
 
f_unlink("record.wav");
u8_sd_fat_status = f_open(&SDFile, "record.wav", FA_CREATE_NEW | FA_READ | FA_WRITE);
for(unsigned char i = 0; i < 10 && u8_sd_fat_status != FR_OK; i++)
{
    HAL_Delay(100);
    u8_sd_fat_status = f_open(&SDFile, "record.wav", FA_CREATE_NEW | FA_READ | FA_WRITE);
}
if(u8_sd_fat_status == FR_OK)
{
    uint16_t u16_array_mic_adc[512];
    uint32_t u32_rec_file_ptr = 0;
    uint32_t u32_i2s_ptr = 22;
 
    f_sync(&SDFile);
    
    HAL_I2S_Receive_DMA(&hi2s2, u32_array_codec_in, sizeof(u32_array_codec_in)/sizeof(uint16_t));
 
    while(u32_rec_file_ptr < 512000)
    {
        UINT u32_i = 0;
 
        u32_i2s_ptr += CodecRead(u16_array_mic_adc, sizeof(u16_array_mic_adc)/sizeof(uint16_t) - u32_i2s_ptr);
 
        if(u32_i2s_ptr >= sizeof(u16_array_mic_adc)/sizeof(uint16_t))
        {
            u8_sd_fat_status = f_write (&SDFile, u16_array_mic_adc, sizeof(u16_array_mic_adc), &u32_i);
            if(u8_sd_fat_status != FR_OK)
            {
                u8_sd_fat_status = f_close(&SDFile);
                if(u8_sd_fat_status != FR_OK)
                    __asm("nop");
                u8_sd_fat_status = f_open(&SDFile, "record.wav", FA_OPEN_ALWAYS | FA_READ | FA_WRITE);
                if(u8_sd_fat_status != FR_OK)
                    __asm("nop");
                u8_sd_fat_status = f_lseek (&SDFile, u32_rec_file_ptr);
                if(u8_sd_fat_status != FR_OK)
                    __asm("nop");
                break;
            }
            f_sync(&SDFile);
        }
        u32_rec_file_ptr += u32_i;
        u32_i2s_ptr = 0;
        }
    }
    f_close(&SDFile);
}

Thanks,

Sin 

4 REPLIES 4

Sounds like the DISKIO layer isn't waiting on the card to complete the write.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks for your reply. But it sounds that I need to go into fatfs driver level. It's not a good news

Just have a look with debugger. The code freeze in disk_write @ ff.c (line 2823). It returns RES_ERROR. But it seems no more detail can be provided

Seems that the data write beyond SD sector block boundary. But I write 1024 bytes each time, which shall not be the case. & this should not be solve by adding delay

ARSL.1
Associate

Hi SSin

I have the same problem as you... when I try to F_Write my Wave data to SDcard it gives me FR_DISK_ERR some times .... Do you found the solution?

Regards

Hello,

I am facing similar error in my application. After few hundreds of successful writes, the FATFS gives me FR_DISK_ERR for f_mount itself. Did you find any solution?