There is that RCC function that you may want to call:
/**
* @brief Select the clock source to output on MCO pin(PA8).
* @note PA8 should be configured in alternate function mode.
* @param RCC_MCOx specifies the output direction for the clock source.
* For STM32G0xx family this parameter can have only one value:
* @arg @ref RCC_MCO1 Clock source to output on MCO1 pin(PA8).
* @param RCC_MCOSource specifies the clock source to output.
* This parameter can be one of the following values:
* @arg @ref RCC_MCO1SOURCE_NOCLOCK MCO output disabled, no clock on MCO
* @arg @ref RCC_MCO1SOURCE_SYSCLK system clock selected as MCO source
* @arg @ref RCC_MCO1SOURCE_HSI HSI clock selected as MCO source
* @arg @ref RCC_MCO1SOURCE_HSE HSE clock selected as MCO sourcee
* @arg @ref RCC_MCO1SOURCE_PLLCLK main PLL clock selected as MCO source
* @arg @ref RCC_MCO1SOURCE_LSI LSI clock selected as MCO source
* @arg @ref RCC_MCO1SOURCE_LSE LSE clock selected as MCO source
* @param RCC_MCODiv specifies the MCO prescaler.
* This parameter can be one of the following values:
* @arg @ref RCC_MCODIV_1 no division applied to MCO clock
* @arg @ref RCC_MCODIV_2 division by 2 applied to MCO clock
* @arg @ref RCC_MCODIV_4 division by 4 applied to MCO clock
* @arg @ref RCC_MCODIV_8 division by 8 applied to MCO clock
* @arg @ref RCC_MCODIV_16 division by 16 applied to MCO clock
* @arg @ref RCC_MCODIV_32 division by 32 applied to MCO clock
* @arg @ref RCC_MCODIV_64 division by 64 applied to MCO clock
* @arg @ref RCC_MCODIV_128 division by 128 applied to MCO clock
* @retval None
*/
void HAL_RCC_MCOConfig(uint32_t RCC_MCOx, uint32_t RCC_MCOSource, uint32_t RCC_MCODiv)
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.