How to configure USB host MSC with CubeMX?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-02-20 6:19 AM
Hello,
I use the STM32F767ZI card and I want to use USB OTG host communication.
For that I tested the program provided by STM32CubeMX, "FatFs_USBDisk". The program worked well.
But when I tried to redo the program using CubeMX. The program compiled. I started the program in debugger mode but couldn't create the file on the USB drive.
Is there a reason that the program generate with CubeMX doesn’t work?
I’m using STM32CubeMX v5 with package STM32Cube_FW_F7_V1.14.0.
Parameter of CubeMX:
RCC -> HSE : BYPASS Clock Souce
LES : Crystal /Ceramic Resonator
SYS -> Serial Wire
Timebase Source : SysTick
Sysclk : 168MHz
USB : 48MHz
USART3 -> Asynchronous
USB_OTG_FS -> Host_Only
Activate_SOF
Activate_VBUS
USB_HOST -> Class for FS IP : Mass Storage Host Class
FATFS -> USB Disk
- Labels:
-
STM32CubeMX
-
STM32F7 Series
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-02-20 9:03 PM
Review the following thread (also comments on the posted code) on how to do the same with STMF4 which should be similar:
https://community.st.com/s/question/0D50X00009Xkdq2SAB/usb-disk-with-cubemx-and-stm32f4discovery
and the referenced blog.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-02-22 12:33 AM
Thank you for your reply.
I read the comments and blog and modified my program. But the program still doesn’t work.
The problem comes from the interrupt settings. The program doesn’t go into the "OTG_FS_IRQHandler" function. This function will say that a USB key is connected.
Moreover, I never go into the functions found in the file "usbh_msc.c".
I changed the level of priority to have the same level as in the example provided by CubeMX but it didn’t change anything. (Command changed: HAL_NVIC_SetPriority (OTG_FS_IRQn, 6, 0)).
Do you have an idea to solve the problem?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-04 2:03 AM
Finally, the problem was solved on its own. I don't know where the problem came from, but following the tutorial provided for STMF4, the program works.
However, I didn't follow the tutorial because I left the heap size at 0x200 and the stack size at 0x400.