2024-11-18 8:04 AM
2024-11-18 8:09 AM - edited 2024-11-18 8:14 AM
Hello @TaehwanChoi and welcome to the community,
As shown by the message you need an internet connection to login.
Then login:
But you need first to create a profile in st.com. or click on Create Account button;
2024-11-20 8:05 AM
Hi. Thank you for reply.
I already have a account.
But, I can't login on MX program yet.
I think it is related to internet connection.
I am connecting to the internet by WiFi.
Just in case, Is connection-way only by Ethernet?
Sincerely,
Taehwan Choi
2024-11-20 8:14 AM
You can connect either with WiFi or Ethernet cable or even 4G/5G.. no matter the media is .. the most important is the internet connection.
Try to check CubeMx internet connection:
then go to Connection parameters and click on "Check Connection". You need to get a green status like shown in the following figure:
Otherwise check your proxy parameters. In that case try to select select "Use System Proxy Parameters".
2024-11-27 7:44 AM
I really would like to use your board(F103-RB).... I don't know why i have a problem....
2024-11-27 7:51 AM
Could you please uninstall that version and install the latest one: V6.13.0
Check if you have a good internet connection. Otherwise you need to check with your IT the proxy parameters.