cancel
Showing results for 
Search instead for 
Did you mean: 

Hardfault memory manager when integrate LVGL into FreeRTOS (FreeRTOS Kernel V10.3.1)

stevenlin3rtwn
Associate

hi all,

Why does the system crash when registering an initialized display driver using lv_disp_drv_register() within “In Register” section? how to replace lv_hal_disp.c for freertos.

1
lv_memset_00(disp, sizeof(lv_disp_t))
After executing the lv_memset_00(disp, sizeof(lv_disp_t)) statement, set the free BlockSize in the BlockLink_t structure to 0 (zero).

then Insert the new block into the list of free blocks (prvInsertBlockIntoFreeList( ( pxNewBlockLink ) )) Due to sufficient space (as subtracting any number from 0 results in a negative number, i.e., a large number), it enters an infinite loop.

2.Create a refresh timer
lv_timer_create(_lv_disp_refr_timer, LV_DISP_DEF_REFR_PERIOD, disp);
why it Add a new head to a linked list to create timer task ?

FreeRTOS Kernel V10.3.1, use heap_4.c
LVGL V8.0.0
board stm32h743

add pvPortRealloc() at heap_4.c

```c

 

void *pvPortRealloc(void *mem, size_t newsize)
{
    if (newsize == 0) {
        vPortFree(mem);
        return NULL;
    }

    void *p;
    p = pvPortMalloc(newsize);
    if (p) {
        /* zero the memory */
        if (mem != NULL) {
            memcpy(p, mem, newsize);
            vPortFree(mem);
        }
    }
    return p;
}

```

 

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Slh
Senior

You should probably increase the TOTAL_HEAP_SIZE in memory management in your RTOS setting and also the Stack size for your task.

hi Slh,

thank your reply.

i have been adjust increase the "heap size", but when 

lv_memset_00(disp, sizeof(lv_disp_t)) // clear lvgl handle struct
After executing the lv_memset_00(disp, sizeof(lv_disp_t)) statement, set the free BlockSize in the BlockLink_t structure to 0 (zero). So ,it not found node to insert or clear free BlockLink size.

```c

lv_disp_t * lv_disp_drv_register(lv_disp_drv_t * driver)

{

lv_disp_t * disp = _lv_ll_ins_head(&LV_GC_ROOT(_lv_disp_ll));

LV_ASSERT_MALLOC(disp);

if(!disp) {

return NULL;

}

 

/*Create a draw context if not created yet*/

if(driver->draw_ctx == NULL) {

lv_draw_ctx_t * draw_ctx = lv_mem_alloc(driver->draw_ctx_size);

LV_ASSERT_MALLOC(draw_ctx);

if(draw_ctx == NULL) return NULL;

driver->draw_ctx_init(driver, draw_ctx);

driver->draw_ctx = draw_ctx;

}

// reset BlockLink_t

lv_memset_00(disp, sizeof(lv_disp_t));

 

disp->driver = driver;

 

disp->inv_en_cnt = 1;

 

lv_disp_t * disp_def_tmp = disp_def;

disp_def = disp; /*Temporarily change the default screen to create the default screens on the

new display*/

/*Create a refresh timer*/

 

// assign invaild value at BlockLink_t struct

disp->refr_timer = lv_timer_create(_lv_disp_refr_timer, LV_DISP_DEF_REFR_PERIOD, disp);

LV_ASSERT_MALLOC(disp->refr_timer);

if(disp->refr_timer == NULL) {

lv_mem_free(disp);

return NULL;

}

 

if(driver->full_refresh && driver->draw_buf->size < (uint32_t)driver->hor_res * driver->ver_res) {

driver->full_refresh = 0;

LV_LOG_WARN("full_refresh requires at least screen sized draw buffer(s)");

}

 

disp->bg_color = lv_color_white();

#if LV_COLOR_SCREEN_TRANSP

disp->bg_opa = LV_OPA_TRANSP;

#else

disp->bg_opa = LV_OPA_COVER;

#endif

 

#if LV_USE_THEME_DEFAULT

if(lv_theme_default_is_inited() == false) {

disp->theme = lv_theme_default_init(disp, lv_palette_main(LV_PALETTE_BLUE), lv_palette_main(LV_PALETTE_RED),

LV_THEME_DEFAULT_DARK, LV_FONT_DEFAULT);

}

else {

disp->theme = lv_theme_default_get();

}

#endif

 

disp->act_scr = lv_obj_create(NULL); /*Create a default screen on the display*/

disp->top_layer = lv_obj_create(NULL); /*Create top layer on the display*/

disp->sys_layer = lv_obj_create(NULL); /*Create sys layer on the display*/

lv_obj_remove_style_all(disp->top_layer);

lv_obj_remove_style_all(disp->sys_layer);

lv_obj_clear_flag(disp->top_layer, LV_OBJ_FLAG_CLICKABLE);

lv_obj_clear_flag(disp->sys_layer, LV_OBJ_FLAG_CLICKABLE);

 

lv_obj_set_scrollbar_mode(disp->top_layer, LV_SCROLLBAR_MODE_OFF);

lv_obj_set_scrollbar_mode(disp->sys_layer, LV_SCROLLBAR_MODE_OFF);

 

lv_obj_invalidate(disp->act_scr);

 

disp_def = disp_def_tmp; /*Revert the default display*/

if(disp_def == NULL) disp_def = disp; /*Initialize the default display*/

 

lv_timer_ready(disp->refr_timer); /*Be sure the screen will be refreshed immediately on start up*/

 

return disp;

}

```

```c

lv_timer_t * lv_timer_create(lv_timer_cb_t timer_xcb, uint32_t period, void * user_data)

{

lv_timer_t * new_timer = NULL;

 

new_timer = _lv_ll_ins_head(&LV_GC_ROOT(_lv_timer_ll));

LV_ASSERT_MALLOC(new_timer);

if(new_timer == NULL) return NULL;

 

new_timer->period = period;

new_timer->timer_cb = timer_xcb;

new_timer->repeat_count = -1;

new_timer->paused = 0;

new_timer->last_run = lv_tick_get();

new_timer->user_data = user_data;

 

timer_created = true;

 

return new_timer;

}

 

 

LV_ATTRIBUTE_FAST_MEM void lv_memset_00(void * dst, size_t len)

{

uint8_t * d8 = (uint8_t *)dst;

uintptr_t d_align = (lv_uintptr_t) d8 & ALIGN_MASK;

 

/*Make the address aligned*/

if(d_align) {

d_align = ALIGN_MASK + 1 - d_align;

while(d_align && len) {

SET8(0);

len--;

d_align--;

}

}

 

uint32_t * d32 = (uint32_t *)d8;

while(len > 32) {

REPEAT8(SET32(0));

len -= 32;

}

 

while(len > 4) {

SET32(0);

len -= 4;

}

 

d8 = (uint8_t *)d32;

while(len) {

SET8(0);

len--;

}

}

```