Skip to main content
PDogu.1
Visitor II
August 29, 2022
Solved

HAL_UART_Receive_IT - how to clean before starting the function

  • August 29, 2022
  • 1 reply
  • 2928 views

Dear Mrs, Mr,

I'm working with a Riverdi discovery board with a STM32. I'm developing a serial protocol for which I'm using interrupt for reception.

  • I enabled the IT in CubeMx
  • Using HAL_UART_Receive_IT(), it is working fine for the first time and also if all characters received are read
  • If I relaunch HAL_UART_Receive_IT() and characters were sent to the uart RX buffer without being read, it fails to work
  • The only way I made it working was to add a HAL_UART_Init function before it and it is working fine.

But I guess this is not the best way to clean buffer, state and pending interrupts. Can you advise of the best way to do it ?

Thank you in advance,

Pascal

This topic has been closed for replies.
Best answer by Guenael Cadier

Hi Pascal,

You could check the ISR (or SR register, depending on the STM32 serie you are using) of UART instance when you execute the 2nd reception (the failing one). Maybe some errors are already present in register, preventing the reception to be properly handled. I'm thinking about the Overrun flag (indicating that some data where received but not read on time from RDR). This could happen if additional data have been received after 1st reception is complete. When this flag is set (some data have been lost), but reception is frozen under the error is cleared.

If this happens in your case, you could clear the flag by resetting flag in ICR (or CR register) prior restarting 2nd reception, for instance using the dedicated macro :

__HAL_UART_CLEAR_FLAG(__HANDLE__, __FLAG__) with UART_CLEAR_OREF as flag.

Regards

Guenael

1 reply

Guenael Cadier
Guenael CadierBest answer
ST Employee
August 30, 2022

Hi Pascal,

You could check the ISR (or SR register, depending on the STM32 serie you are using) of UART instance when you execute the 2nd reception (the failing one). Maybe some errors are already present in register, preventing the reception to be properly handled. I'm thinking about the Overrun flag (indicating that some data where received but not read on time from RDR). This could happen if additional data have been received after 1st reception is complete. When this flag is set (some data have been lost), but reception is frozen under the error is cleared.

If this happens in your case, you could clear the flag by resetting flag in ICR (or CR register) prior restarting 2nd reception, for instance using the dedicated macro :

__HAL_UART_CLEAR_FLAG(__HANDLE__, __FLAG__) with UART_CLEAR_OREF as flag.

Regards

Guenael