cancel
Showing results for 
Search instead for 
Did you mean: 

in new stm32cubeIDE "ctrl+space" delay 20 sec!!!

kshin.111
Associate III

hi

after uninstalling:

"en.st-stm32cubeide_1.9.0_12015_20220302_0855_x86_64.exe_v1.9.0"

"en.stm32cubemx-win_v6-5-0_v6.5.0"

"en.stm32cubeprg-win64_v2-10-0_v2.10.0"

and installing:

"en.stm32cubemx-win_v6-6-1"

"en.stm32cubeprg-win64_v2-11-0"

"en.st-stm32cubeide_1.10.1_12716_20220707_0928_x86_64.exe"

in stm32cubeIDE any time push "ctrl+space" for autocomplete, working but after delay for 20 second ! :o

and into 20 second, stm32cubeIDE is hang.

example:

"uint8" now press ctrl+space and after 20 seconds it will show uint8_t and other words...

please help me

---

my pc information:

Processor: Intel(R) Core(TM) i7-7700K CPU

RAM: 16GB

System type   64-bit operating system, x64-based processor

Graphic card: NVIDIA GeForce GTX 1060 6GB

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Diane POMABIA
ST Employee

Hi @kshin.11​ ,

I have the same Environment Cube as you but I don't have this problem, can you see in your Task Manager, if your Pc is not running other programs, which can explain this delay? Do you always have the same problem when you restart your PC?

Regards , 

Diane 

Semer CHERNI
ST Employee

Hello @kshin.11​ 

Try to create a new workspace. If issue resolved you should try to delete the .pdom files under the work space repo %(workspace)\.metadata\.plugins\org.eclipse.cdt.core\*.pdom

Kind regards,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Semer CHERNI
ST Employee

Hello @kshin.11​ 

Do you still have the delay issue with the CubeIDE tool?

Kind regards,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.