cancel
Showing results for 
Search instead for 
Did you mean: 

FreeRTOS not available in latest CubeMX?

Ricko
Senior III

Hi,

I just updated CubeIDE/CubeMX, and after creating a new project, I began configuring the microcontroller. However, when I tried to install FreeRTOS, it didn’t seem to be available. In the older version of CubeMX, there was a FreeRTOS option under Middleware (as shown in the first screenshot from a video), but it appears to be missing now.

I did find X-CUBE-FREERTOS, but it doesn’t seem to offer any options like CMSIS_V1 or CMSIS_V2.

1. Could someone clarify what happened? What exactly is X-CUBE-FREERTOS, and is it now the only or perhaps the preferred option? If not, how can I install FreeRTOS?

2. How do I select CMSIS_V1 or CMSIS_V2 and all other parameters like in the older configurator (shown in the third screenshot)?

3. Additionally, are all ST libraries that rely on FreeRTOS now using X-CUBE-FREERTOS?

Thanks you as always! :)

Ricko

 

 

Ricko_2-1741046826671.png

 

 

Ricko_0-1741046681156.png

 

 

 

Ricko_0-1741049461926.png

 

 

 

 

0 REPLIES 0