cancel
Showing results for 
Search instead for 
Did you mean: 

Different FreeRTOS in latest CubeMX?

Ricko
Senior III

Hi,

I just updated CubeIDE/CubeMX, and after creating a new project, I began configuring the microcontroller. However, when I tried to install FreeRTOS, it didn’t seem to be available. In the older version of CubeMX, there was a FreeRTOS option under Middleware (as shown in the first screenshot from a video), but it appears to be missing now. I did find X-CUBE-FREERTOS, but it doesn’t seem to offer any options like CMSIS_V1 or CMSIS_V2 or any  ther very many parameters that FreeRTOS that in the previous version were available.

What happened?

1. Is that X-CUBE-FREERTOS, the only or perhaps the preferred option to use/install hrough MX?

2. How do I select CMSIS_V1 or CMSIS_V2 and all other parameters like in the older configurator (third screenshot)?

3. Are all ST libraries that rely on FreeRTOS now using X-CUBE-FREERTOS?

Thanks you  :)

Ricko

 

 

Ricko_2-1741046826671.png

 

 

Ricko_0-1741046681156.png

 

 

 

Ricko_0-1741049461926.png

 

 

 

 

0 REPLIES 0