2023-01-31 5:03 AM
I am running STM32CubeIDE Version: 1.11.2 Build: 14494_20230119_0724 (UTC). When I startup CubeIDE, I am seeing the following error in the Error Log:
"CubeMX plugin appears to be active, Log4j initialization might be too late."
I would appreciate it if someone could point me in the correct direction to resolve it (or ignore it). I am relatively new to CubeIDE, as I have primarily been doing my STM32 work from the command line with Makefiles. CubeIDE seems to be working fine so the error is not slowing me down at the moment.
2023-01-31 5:04 AM
Additional information from the log file:
eclipse.buildId=Version 1.11.2
java.version=11.0.16
java.vendor=Eclipse Adoptium
BootLoader constants: OS=win32, ARCH=x86_64, WS=win32, NL=en_US
Command-line arguments: -os win32 -ws win32 -arch x86_64
2023-02-01 8:37 AM
Hello @BHime
First let me thank you for posting.
Could you provide the complete log files found under the "workspace\.metadata" directory:
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-01 9:35 AM
2023-02-01 9:35 AM
2023-02-01 9:36 AM
2024-02-28 5:03 AM
Hello,
I encounter the same error. Not sure what happened? I am using stm32cubeide 1.14.1
2024-04-06 10:24 AM
Any solution on this problem?!, I have the same error message...
2024-04-11 1:03 PM
I have the same problem. Any solution yet?
2024-11-07 4:46 AM
I encounter the same error. I am using stm32cubeide 1.16.1