cancel
Showing results for 
Search instead for 
Did you mean: 

Error downloading FW.F1.1.7.0 MCU package

Dmitri
Associate II

Hi,

recently I installed STM32CubeMX. When I click 'Check for update' menu item 'STM32CubeF1 Firmware Package V1.7.0 / 09-October-2018' is shown. But when I press 'Install Now' the following error happens:

In the log I see:

2018-11-20 23:56:39,197 [ERROR] ServerAccessManage:919 - Problem, file not found on Server

2018-11-20 23:56:39,197 [ERROR] ServerAccessManage:491 - Problem, file not found on Server : stm32cube_fw_f1_v170.zip.

Is v1.7.0 package available to download?

thanks,

Dmitri

12 REPLIES 12

ST looks to have got a bit ahead of themselves, issue from here also, expect it to be resolved shortly. ​ @Khouloud GARSI​ 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi @Dmitri​ ,

Issue confirmed from our side and highlighted internally.

Sorry for this inconvenience. This will be fixed ASAP!

Khouloud.

Houda GHABRI
ST Employee

Hello @Dmitri​ 

Thanks for your feedback.

FW F1 1.7.0 will be available Tomorrow after doing a refresh in update Manager.

Sorry for the inconvenience.

Best regards,

Houda

Khouloud GARSI
Lead II

Hi @Dmitri​ ,

Issue solved: The STM32F1 v1.7.0 is now available for download.

Khouloud.

Confirmed, have it mirrored if anyone needs it, or the other releases. The F7.1.13.0 was 1.2GB!!

ST should really consider hosting torrents for those on lower bandwidth connections, download limits or those who have intermittent connections which might benefit from a restartable download, ie continue rather than start over...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks for quick response!

You're always welcome!

Still having this problem. Can you provide a mirror? Thanks

https://drive.google.com/open?id=1-2PM2qaXjtyD7KqJ6tsvp-l0EeAPqjbo

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..