cancel
Showing results for 
Search instead for 
Did you mean: 

Does SD work with CubeMX 5.6.1? (STM32F411/STM32F412)?

MarieMaurer
Associate III

I have found an old video

https://www.youtube.com/watch?v=0NbBem8U80Y

telling CubeMX 4.24 and 4.23 had a bug with SDIO, 4 bit mode, DMA.

It seems for them 4.21 worked.

I am using newest CubeMX 5.6.1. When was bug fixed? I assume it was fixed also in version 5.6.1?

I first started on a STM32F412, meanwhile on a Nucleo Evalboard with STM32F411,

but I can't seem to be able to access SD card. I see CLK line toggling. I see bits on CMD

(recorded with a logic analyzer)

but can't interpret them. I assume SD card is not answering at all, because makes

not much difference if card is in or not. It is a 32GB uSD.

I have no pullup. Do I need (external/internal) pull ups to get it working?

I want to work without interrupt, and also without DMA, to make it easier.

Is it possible? Is looks like I can't disable "Use dma template" in FatFS dialog.

I don't have a detect pin, just select no pin and ignore warning.

I can't switch power, 3.3V for uSD card is always on. Is this a problem?

Does someone have a working project with source code, so I can adapt, try out and compare? I can use STM32F411 and also STM32F412, but with first one I am more flexible.

I am using arm-gcc in WSL with latest Ubuntu.

Dont know if helpful, this is what I logged out:

[    0.000][p][Task] sizeof(FATFS)=564
[    0.000][p][Task] sizeof(FIL)=560
[    0.000][p][Task] In f_open Pos 1
[    0.000][p][Task] In f_open Pos 2
[    0.000][p][Task] In find_volume Pos 1
[    0.000][p][Task] In find_volume Pos 3
[    0.000][p][Task] In find_volume Pos 4
[    0.000][p][Task] In find_volume Pos 5
[    0.000][p][Task] In disk_initialize
[    0.000][p][Task] I am in SD_initialize
[    0.000][p][Task] I am in SD_initialize Pos 2
[    0.000][p][Task] I am in SD_initialize Pos 3
[    0.000][p][Task] I am in BSP_SD_Init Pos 1
[    0.000][p][Task] I am in BSP_SD_Init Pos 2
[    0.000][p][Task] I am in HAL_SD_Init Pos 1
[    0.000][p][Task] I am in HAL_SD_Init Pos 2
[    0.000][p][Task] I am in HAL_SD_Init Pos 3
[    0.000][p][Task] I am in HAL_SD_InitCard Pos 1
[    0.000][p][Task] I am in HAL_SD_InitCard Pos 3
[    0.000][p][Task] I am in HAL_SD_InitCard Pos 4
[    0.000][p][Task] I am in SD_PowerON
[    0.000][p][Task] I am in SDIO_SendCommand Argument=00000000 CmdIndex=00000000 Response=00000000 WaitForInterrupt=00000000 CPSM=00000400
[    0.000][p][Task] I am in SDMMC_GetCmdError
[    0.000][p][Task] I am in SDMMC_GetCmdError -> SDMMC_ERROR_NONE
[    0.000][p][Task] I am in SD_PowerON Pos 2
[    0.000][p][Task] I am in SDMMC_CmdOperCond
[    0.000][p][Task] I am in SDIO_SendCommand Argument=000001aa CmdIndex=00000008 Response=00000040 WaitForInterrupt=00000000 CPSM=00000400
[    0.000][p][Task] I am in SDMMC_CmdOperCond Pos 2
[    0.000][p][Task] I am in SDMMC_GetCmdResp7 SystemCoreClock=72000000 count=45000000
[    0.000][p][Task] I am in SDMMC_GetCmdResp7 -> SDMMC_ERROR_CMD_RSP_TIMEOUT
[    0.000][p][Task] I am in SD_PowerON Pos 3
[    0.000][p][Task] I am in SDIO_SendCommand Argument=00000000 CmdIndex=00000000 Response=00000000 WaitForInterrupt=00000000 CPSM=00000400
[    0.000][p][Task] I am in SDMMC_GetCmdError
[    0.000][p][Task] I am in SDMMC_GetCmdError -> SDMMC_ERROR_NONE
[    0.000][p][Task] I am in SD_PowerON Pos 5
[    0.000][p][Task] I am in SD_PowerON Pos 9
[    0.000][p][Task] I am in SD_PowerON Pos 10
[    0.000][p][Task] I am in SDMMC_CmdAppCommand
[    0.000][p][Task] I am in SDIO_SendCommand Argument=00000000 CmdIndex=00000037 Response=00000040 WaitForInterrupt=00000000 CPSM=00000400
[    0.000][p][Task] I am in SDMMC_CmdAppCommand Pos 2
[    0.000][p][Task] I am in SDMMC_GetCmdResp1
[    0.000][p][Task] I am in SDMMC_GetCmdResp1 -> SDMMC_ERROR_NONE
[    0.000][p][Task] I am in SD_PowerON Pos 12
[    0.000][p][Task] I am in SDIO_SendCommand Argument=c1100000 CmdIndex=00000029 Response=00000040 WaitForInterrupt=00000000 CPSM=00000400
[    0.000][p][Task] I am in SD_PowerON Pos 14
[    0.000][p][Task] I am in SD_PowerON Pos 15
[    0.000][p][Task] I am in SD_PowerON Pos 16 validvoltage=0 count=0
[    0.000][p][Task] I am in SD_PowerON Pos 10
[    0.000][p][Task] I am in SDMMC_CmdAppCommand
[    0.000][p][Task] I am in SDIO_SendCommand Argument=00000000 CmdIndex=00000037 Response=00000040 WaitForInterrupt=00000000 CPSM=00000400
[    0.000][p][Task] I am in SDMMC_CmdAppCommand Pos 2
[    0.000][p][Task] I am in SDMMC_GetCmdResp1
[    0.000][p][Task] I am in SDMMC_GetCmdResp1 -> SDMMC_ERROR_CMD_RSP_TIMEOUT
[    0.000][p][Task] I am in SD_PowerON Pos 11
[    0.000][p][Task] I am in HAL_SD_InitCard Pos 5
[    0.000][p][Task] I am in HAL_SD_Init Pos 4
[    0.000][p][Task] I am in BSP_SD_Init Pos 5
[    0.000][p][Task] I am in SD_initialize Pos 7
[    0.000][p][Task] I am in SD_initialize Pos 16
[    0.000][p][Task] In f_open Pos 12
[    0.000][p][Task] In f_open Pos 13
[    0.000][p][Task] After f_open fr=3
[    0.000][p][Task] FatFS: before call f_close
[    0.000][p][Task] FatFS: after call f_close
[    0.000][p][Task] Test fat fs done
 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Generally the way the forums work, we only hear bad news. If I believed the forum I'd assume nothing with CubeMX worked properly.

Polled operation on the F4 should be viable. DMA should also be viable, needs 32-bit (4-byte) aligned buffers.

Should be several working examples for EVAL and DISCO boards in the CubeF4 repository, often in the Applications\FatFs directories for boards shipping with SD card sockets.

Pull-up of data/command pins at the socket is generally recommended. Lacking them I'd use the internal ones.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..