cancel
Showing results for 
Search instead for 
Did you mean: 

Different FreeRTOS in latest CubeMX?

Ricko
Senior III

Hi,

I just updated CubeIDE/CubeMX, and after creating a new project, I began configuring the microcontroller. However, when I tried to install FreeRTOS, it didn’t seem to be available. In the older version of CubeMX, there was a FreeRTOS option under Middleware (as shown in the first screenshot from a video), but it appears to be missing now. I did find X-CUBE-FREERTOS, but it doesn’t seem to offer any options like CMSIS_V1 or CMSIS_V2 or any  ther very many parameters that FreeRTOS that in the previous version were available.

What happened?

1. Is that X-CUBE-FREERTOS, the only or perhaps the preferred option to use/install hrough MX?

2. How do I select CMSIS_V1 or CMSIS_V2 and all other parameters like in the older configurator (third screenshot)?

3. Are all ST libraries that rely on FreeRTOS now using X-CUBE-FREERTOS?

Thanks you  :)

Ricko

 

 

Ricko_2-1741046826671.png

 

 

Ricko_0-1741046681156.png

 

 

 

Ricko_0-1741049461926.png

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @Ricko ,

In answer to your question, Some STM32 series support Freertos and others support X-Cube-Freertos.
With Freertos, users can select either CMSIS V1 or CMSIS V2.
Whereas with x-cube-freertos , CMSIS RTOS 2 is set as default.

 

Thanks.

Mahmoud

View solution in original post

5 REPLIES 5
Mahmoud Ben Romdhane
ST Employee

Hello @Ricko ,

 

First let me thank you for posting.

You need to enable X-CUBE-FREERTOS in STM32CubeMX:

Click [Select Components] under the [Software Packs] menu.

Scroll down in the list and select [ST Microelectronics.X-CUBE-FREERTOS]. In case it is not installed, or you would need to use a different version, install it first using the [Install] button within the [Selection] column.

 

MahmoudBenRomdhane_0-1741160778303.png

MahmoudBenRomdhane_1-1741160824063.png

 

I suggest also that you take a look at this article: How to use STM32U5 with FreeRTOSâ„¢ in tickless mode - STMicroelectronics Community

 

Thanks.

Mahmoud

Hello @Ricko ,

In answer to your question, Some STM32 series support Freertos and others support X-Cube-Freertos.
With Freertos, users can select either CMSIS V1 or CMSIS V2.
Whereas with x-cube-freertos , CMSIS RTOS 2 is set as default.

 

Thanks.

Mahmoud

Thank you @Mahmoud Ben Romdhane 

what is the difference (generally and in API)?

Where can I find a document or video explaining the difference?

Thank you :)

Hello @Ricko ,

 

I recommend that you consult this Data Brief and those Videos.

 

Thanks.

Mahmoud

 

Thank you @Mahmoud Ben Romdhane  :)