CubeMx version v6.9.0 deleting my folder structure/ Middleware
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-07-26 6:48 AM - last edited on ‎2023-08-03 8:01 AM by KDJEM.1
CubeMx version v6.9.0 deleting my folder structure/ Middleware.
I tried to generate code via v6.9.0 and it just deletes my entire middleware files. My all commits are gone.
- Labels:
-
STM32WL series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-02 3:24 AM
Hello @Aanchal and welcome to the community :),
Which toolchain/IDE are you using for generation project? Are you using MDK-ARM?
Could you please download and use the latest version of STM32CubeMX6.9.1.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-03 5:50 AM
No the issue is not resolved facing issue related to this file #include "cmsis_os2.h".
../Drivers/VVG_OS\VVG_OS_Thread.h(10): error: 'cmsis_os2.h' file not found
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-03 6:28 AM
Hi @Aanchal ,
Could you please precise:
-Which toolchain/IDE are you using for generation project?
-Which STM32 product are you using?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-03 6:44 AM
-Which toolchain/IDE are you using for generation project? - i am using keil version 5
-Which STM32 product are you using? - stm32wl55cc
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-04 3:57 AM - edited ‎2023-08-04 4:01 AM
Hello @Aanchal ,
I made some test with STM32WL55CCU6 using STM32CubeMX6.9.1 and I can't reproduce the issue.
Please make sure that after adding the user file in your project generated by Keil, to click on File--> save all ( this step is very important ) then when you regenerate the code using STM32CubeMX 6.9.1 the added user file will not be deleted .
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-25 2:23 AM
Hello @KDJEM.1 ,
i have the same problem since several versions of STM32CubeIDE. At the moment I'm using version 1.13.1 and the problem ist still there.
I'm using a H743ZG with RTOS activated. In the automatically generated Folder "/Middlewares/" I added some linked folders and they are not deleted. But I also added a Folder named "System" and this folder is always deleted if I regenerate the code.
There should be two internal Tickets: 147368, 151040. Could you reproduce the issue.
Best regards
Jens
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-25 6:15 AM
Hello @JensH ,
147368 ticket reported STM32CubeMx v6.8.0 deletes Folder added by user when regenerate the code using MDK-ARM issue. This issue is already solved in STM32CubeMX6.9.1 version.
151040 ticket reported STM32CubeMX deletes manually added folders "Utilities" or "Middlewares" (same folder name reserved by Cube MX). This issue will be solved in the coming release.
To reproduce your issue, could you please describe the steps to follow?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-25 6:36 AM
Hi @KDJEM.1 ,
it seems to be the same problem as 151040.
To reproduce the issue:
- Generate a Project in STM32Cube IDE including Azure RTOS packages
- A folder named "Middelwares" will be created
- Adding a new sub folder named "System" to "Middlewares"
- Open the *.ioc file and do some editing
- regenerate the project and the "System" folder will be deleted
I hope this explanation helps. Best regards
Jens
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-20 6:38 AM
Hello
I have a similar issue. Using latest version of CubeMX: 6.9.2 with last L4 Firmware Package: 1.18
I'm using the default B-L462E-CELL1 demoboard project with some modifications. Each time I generate with CubeMX, it remove completely the Utilities directory. It seems that directories in Middleware are not removed.
Expected beavior: CubeMX do not touch to directories!