2024-07-16 7:36 AM
hello!
I start this post because i have created a new project with CUBEMX 6.12.0 and i am having some issues.
When I generate code without THREAD X activated, the generation is completed without any error. However, when I add the thread X option (see .ioc file), the generation process gets stuck in "copying files"
I am developing a project for an STM32H563xxx HW and I have updated all the necessary libraries such as:
How is that? What can I do to solve this problem.
2024-07-17 3:36 AM
Hello @massimoperdigo
First let me thank you for posting.
Actually I was capable to generate the project using your IOC without getting stuck in "copying files" of course i used CubeMX 6.12.0.
So let's try to uninstall and then reinstall CubeMX 6.12.0 , this could help resolve the issue .
THX
Ghofrane
2024-07-17 3:44 AM
Hi, good morning.
I did it already and it does not work. Do I need external packages or smthing else?
ty