2024-01-08 02:22 PM
In CubeMX when configuring a SPI peripheral I can only choose either 8 or 16 bit, but the STM32G491 reference manual says data size can be from 4 to 16 bit. Is this a bug in CubeMX?
(using the newest CubeMX version)
Solved! Go to Solution.
2024-01-09 01:54 AM
STM32G491xC ds :
But in Cube can only select 8 or 16 bits, i can confirm.
Obviously a bug.
@Ghofrane GSOURI , would you report this ?
2024-01-09 12:43 AM
Hello @decalvus
First let me thank you for posting.
The data size selection in SPI is important because it determines the resolution and range of values that can be transmitted in a single communication transaction. Here's an explanation of the different data size options:
1- 4-bit data size: With a 4-bit data size, each data element transferred during an SPI transaction is represented using 4 bits. This allows for a range of values from 0 to 15 (2^4 - 1). A 4-bit data size is less common but can be useful in certain applications where limited precision is required, or when the transmitted data is compact and can be represented within a small range.
2- 8-bit data size: An 8-bit data size is the most common option in SPI. Each data element is represented using 8 bits, allowing for a range of values from 0 to 255 (2^8 - 1). This is typically sufficient for most applications and provides a good balance between precision and data size.
3- 16-bit data size: A 16-bit data size allows for even larger values to be transmitted. Each data element is represented using 16 bits, providing a range of values from 0 to 65,535 (2^16 - 1). This data size option is useful when dealing with larger data values or when higher precision is required.
Indeed, for most applications, the 8-bit and 16-bit data sizes in SPI are sufficient and cover the majority of use cases. The 8-bit data size provides a good balance of precision and data size, while the 16-bit data size offers a wider range of values and higher precision and that's why CubeMX offer those two options .
Thx
Ghofrane
2024-01-09 01:54 AM
STM32G491xC ds :
But in Cube can only select 8 or 16 bits, i can confirm.
Obviously a bug.
@Ghofrane GSOURI , would you report this ?
2024-01-09 05:11 AM
Thank you for your contributions and for your detailed explanations,
I confirm the issue on my side, it has been reported to STM32CubeMX development team .
Internal ticket number: 170304(This is an internal tracking number and is not accessible or usable by customers).
I will keep you posted with update
Ghofrane
2024-01-09 07:14 AM
Hi Ghofrane
Thanks for helping.
Did you acknowledge it as a ‘bug’ in CubeMX? (I’m a bit unsure since you replied “and that's why CubeMX offer those two options”)
Also, the datasheet mentions the range is from 4 to 16 bits (4,5,6…16), not only 4, 8 or 16 bits.