2024-05-16 08:00 AM - edited 2024-05-17 09:15 PM
As can be seen from screenshots, cubemx displays the space as "ft" and the whole interface is hard to read. Version v6.11.1 and v6.9.0 have this issue and v6.5.0 does not. This issue is only on Linux(fedora 40). All those three versions work very well on Windows. Thanks
2024-06-03 01:10 AM
Hello @greghuang
First let me thank you for posting.
I am in the process of checking this and will return to you as soon as possible.
THX
Ghofrane
2024-06-03 01:25 AM
Hello @greghuang
After checking the UM1718 :3.1.1 Supported operating systems and architectures
• Windows® 10 and 11, 64-bit (x64)
• Linux®: Ubuntu® LTS 20.04 and LTS 22.04, and Fedora® 37
• macOS® 13 (Ventura), macOS® 14 (Sonoma)
THX
Ghofrane