2018-09-10 11:20 PM
Below images show a PCC step configuration window and my clock tree configuration. As seen i can not change info under clock tab of PCC. Anybody know the reason ?
2018-10-08 6:37 AM
Hello,
Please note that if you select "Scale3-Low", you will be able to enter the value of the frequency in "User Choice" field. In this case, you need to select first "User-defined" as CPU Frequency.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-10-09 12:14 AM
Hello Amel,
Thanks for your time ! In the case i select "Scale3-Low", CPU freq is selectable but i still cannot specify Clock Source frequency. It is fixed to 4 MHz. Doesn't Clock Source frequency affect power consumption ? I plan to use 20 MHz crystal by the way.
2018-10-25 2:08 AM
Hi,
The PCC clock is independent form your project configuration.
We are working on synchronizing this tool and it will be available in a next release with all clock configurations