CubeMX integration with BSP drivers
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-19 10:52 AM
I have been using the CubexMX for a few years and have no problems with programming nucleo and discovery boards.
I am using Keil IDE.
I recently bough the
http://www.st.com/en/ecosystems/x-nucleo-iks01a1.html
and have some problems with integration it with nucleo-F411.===
Starting with the library description and trying to understand all the dependencies seems to be daunting task.
I tried it but I found it difficult to solve library dependencies issues. I am not talking about what function to call - it's rather inter library dependencies issues.
===
Opening already existing example project for F401 and replacing the MCU with F411 gives so many compilation errors so I rejected the idea for now.
===
I wonder if someone have some experience how to quickly integrate the CubeMX-generated program skeleton with BSP drivers. The goal is to have compilation/linking error free application skeleton.
The Getting started document for x-nucleo boards is focused on general ideas of the HAL and BSP layers.
I am looking for more practical approach of integrating BSP with Cubex.
Thanks for any suggestion,
Bogdan
#bsp #cube-mxSolved! Go to Solution.
- Labels:
-
STM32CubeMX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-01 10:12 AM
Hi Sirma,
Thank you for your effort.
What you have prepared always works as you do not call any MEMs API in your project. It's pure app skeleton - no api is called. No issues then.
===
The fun begins when you try to call any API e.g. BSP_TEMPERATURE_Init( HTS221_T_0, &HTS221_T_0_handle )
When you add required include files (#include 'x_nucleo_iks01a1.h', #include 'x_nucleo_iks01a1_temperature.h', etc).
At some point you get:
*** Using Compiler 'V5.06 update 4 (build 422)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'
Build target 'F401-MEMs'compiling x_nucleo_iks01a1.c.....\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(62): error: #20: identifier 'I2C_HandleTypeDef' is undefined static I2C_HandleTypeDef I2C_EXPBD_Handle;..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(286): warning: #223-D: function 'HAL_I2C_GetState' declared implicitly if(HAL_I2C_GetState( &I2C_EXPBD_Handle) == HAL_I2C_STATE_RESET )..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(286): error: #20: identifier 'HAL_I2C_STATE_RESET' is undefined if(HAL_I2C_GetState( &I2C_EXPBD_Handle) == HAL_I2C_STATE_RESET )..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(293): error: #20: identifier 'I2C_DUTYCYCLE_2' is undefined I2C_EXPBD_Handle.Init.DutyCycle = I2C_DUTYCYCLE_2;..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(304): error: #20: identifier 'I2C_ADDRESSINGMODE_7BIT' is undefined I2C_EXPBD_Handle.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(309): warning: #223-D: function 'HAL_I2C_Init' declared implicitly HAL_I2C_Init( &I2C_EXPBD_Handle );..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(312): warning: #223-D: function 'HAL_I2C_GetState' declared implicitly if( HAL_I2C_GetState( &I2C_EXPBD_Handle) == HAL_I2C_STATE_READY )..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(312): error: #20: identifier 'HAL_I2C_STATE_READY' is undefined if( HAL_I2C_GetState( &I2C_EXPBD_Handle) == HAL_I2C_STATE_READY )..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(338): warning: #223-D: function 'HAL_I2C_Mem_Write' declared implicitly status = HAL_I2C_Mem_Write( &I2C_EXPBD_Handle, Addr, ( uint16_t )Reg, I2C_MEMADD_SIZE_8BIT, pBuffer, Size,..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(338): error: #20: identifier 'I2C_MEMADD_SIZE_8BIT' is undefined status = HAL_I2C_Mem_Write( &I2C_EXPBD_Handle, Addr, ( uint16_t )Reg, I2C_MEMADD_SIZE_8BIT, pBuffer, Size,..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(338): warning: #188-D: enumerated type mixed with another type status = HAL_I2C_Mem_Write( &I2C_EXPBD_Handle, Addr, ( uint16_t )Reg, I2C_MEMADD_SIZE_8BIT, pBuffer, Size,..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(371): warning: #223-D: function 'HAL_I2C_Mem_Read' declared implicitly status = HAL_I2C_Mem_Read( &I2C_EXPBD_Handle, Addr, ( uint16_t )Reg, I2C_MEMADD_SIZE_8BIT, pBuffer, Size,..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(371): error: #20: identifier 'I2C_MEMADD_SIZE_8BIT' is undefined status = HAL_I2C_Mem_Read( &I2C_EXPBD_Handle, Addr, ( uint16_t )Reg, I2C_MEMADD_SIZE_8BIT, pBuffer, Size,..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(371): warning: #188-D: enumerated type mixed with another type status = HAL_I2C_Mem_Read( &I2C_EXPBD_Handle, Addr, ( uint16_t )Reg, I2C_MEMADD_SIZE_8BIT, pBuffer, Size,..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c(399): warning: #223-D: function 'HAL_I2C_DeInit' declared implicitly HAL_I2C_DeInit( &I2C_EXPBD_Handle );..\Drivers\BSP\X_NUCLEO_IKS01A1\x_nucleo_iks01a1.c: 8 warnings, 7 errorscompiling main.c...'F401-MEMs\F401-MEMs.axf' - 7 Error(s), 8 Warning(s).Target not created.==================Anyway, I gave up. I spent too much time on this. It seems too difficult to use MEMs board for me.
Thank you for your effort.
Bogdan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-01 10:35 AM
Hello Bogdan,
The main concept is that the BSP corresponding to the extension boards needs to be copied into the drivers directory.
I did the following to make it compilable under Eclipse:
- Create a project with CubeMX
- Download the IKS01A1 zip from this page:
- expand the zip and copy this BSP directory (en.x-cube-mems1\STM32CubeExpansion_MEMS1_V3.0.0\Drivers\BSP) into the Drivers directory generated by CubeMX
- Then I had to add USE_STM32F4XX_NUCLEO in Preprocessor settings (Project->Properties->C/C++ Build->Settings->Tools Settings ->Preprocessor)
- I had to add all new includes from BSP : BSP/Components/Common,hts221,lis3mdl,lps22hb,lps25hb, lsm6ds0, lsm6ds3, lsm6dsl, lsm303agr (Project->Properties->C/C++ Build->Settings->Tools Settings ->Includes)
- Then clean and build
This built well in my machine.
You have to see the BSP as an HAL upper layer, to help on this IKS01A1 board.
Hope it help.
Kind regards
Sirma
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-01 2:44 PM
Hi Sirma / Eric,
I tried again and I think I found the final solution:
I. Follow your procedure but point 1) shall be changed to:
Create a project with CubeMX and enable I2C1 because the BSP drivers will use it
This way you will eliminate all I2C related error
II. Include the following files in your main.c
#include 'x_nucleo_iks01a1.h'
#include 'x_nucleo_iks01a1_temperature.h'#include <string.h>#include <math.h>Note :string.h and math.h are required because I reused an example function.
III. Add the pointers required by MEM APIe.g. for temperature sensor:
static void *HTS221_T_0_handle = NULL;
IV. Use API for example:
BSP_TEMPERATURE_Init( HTS221_T_0, &HTS221_T_0_handle ); BSP_TEMPERATURE_Sensor_Enable( HTS221_T_0_handle ); Temperature_Sensor_Handler( HTS221_T_0_handle ); BSP_TEMPERATURE_Sensor_Disable( HTS221_T_0_handle );I reused Temperature_Sensor_Handler( HTS221_T_0_handle ); for simplicity
V. Copy the example function to main.c:
static void Temperature_Sensor_Handler( void *handle )
{...
}
VI. Add required *.C files to your project (in this case *.C files from the drivers folders e.g. in my case
<FileName>x_nucleo_iks01a1_temperature.c</FileName> <FileName>HTS221_Driver.c</FileName> <FileName>HTS221_Driver_HL.c</FileName> <FileName>x_nucleo_iks01a1.c</FileName> <FileName>LPS22HB_Driver.c</FileName> <FileName>LPS22HB_Driver_HL.c</FileName> <FileName>LPS25HB_Driver.c</FileName> <FileName>LPS25HB_Driver_HL.c</FileName>===
Summary: It seems that CubeMX and MEMs BSP can be easly integrated.
The general idea is:
-generate CubeMX and enable required resources. In case of MEMs it's I2C1, In case of L476G (Eric's example) it's
DFSDM1
-add include search paths to your project
-add *.C files from Drivers folders to satisfy linker
-then work with the API
===
Sirma/Eric,
Thank you very much for great support.
Bogdan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-05 12:34 PM
Why cant CudeIDE add the BSP folder anyway? Just a few MBs.
Until there is a better solution, just add the BSP folder when generating projects by CubeIDE together with the include paths and linker paths.
This way we can reduce the problems and confusions.
Copy here, copy there, add paths to this and that.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-06 6:48 PM
Why cant just copy the whole BSP folder and add in the include paths and also symbols.
The folder is just few MBs.
This way it wont create any confusion among newbie like me.

- « Previous
-
- 1
- 2
- Next »