cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX hanging in generating code...

Ryan213
Associate II

I'm freezing on the following screen, is there anything I can do?

Ryan213_0-1740532773650.png

TK

1 ACCEPTED SOLUTION

Accepted Solutions
kurtmicke
Associate

Thanks for info. In fact I got it to work today. I did two things:

1. Deleting .\Users\<username> and delete .stm32cubemx folder. Got the idea from Reddit...

After this I tested, no difference.

2. Filling in project name and location.

Tested again, Da da! working,

So probably the problem was on top of the keyboard.

View solution in original post

6 REPLIES 6
STTwo-32
ST Employee

Hello @Ryan213 and welcome to the ST Community. 
Could you try to uninstall and reinstall it or at least restart your PC.

PS: make sure that you are using the last version of the STM32CubeMX. (V6.13.0)

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I've reinstall and upgraded to version 16.4, but I'm still stuck on the following screen.

Ryan213_0-1741065421850.png

 

 

Ryan213_1-1741065421623.png

 

Is there anything else I can try? Or if the CubeIDE has this feature built in.

Hello I have exactly the same problem. Installed latest version yesterday. Have you been able to solve the problem?

BR Micke

If you have just upgraded then the first time you open your .ioc you will be prompted to migrate to the new version (or not). Maybe worth checking that you have not overlooked that popup window which may appear on another screen if you have a second connected to your PC.

kurtmicke
Associate

Thanks for info. In fact I got it to work today. I did two things:

1. Deleting .\Users\<username> and delete .stm32cubemx folder. Got the idea from Reddit...

After this I tested, no difference.

2. Filling in project name and location.

Tested again, Da da! working,

So probably the problem was on top of the keyboard.

Its work!
thank you  kurtmicke .