cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 6.12.0 on MacOS has a difficult install then incorrect permissions

I just installed 6.12.0 on my MacOS 14.5 system.

First, the updater requires administrative privileges, which is not a thing, so you have to fire up a terminal session, cd into the 6.11.0 application bundle to just the right place, sodo execute the application... and throw stones at Windows for imputing their weird user experience expectations on the world.

Anyway, once you finally get everything installed and generate code, you get:

Screenshot 2024-07-05 at 12.18.56.png

 

Indeed the directory in question is:

drwxr-xr-x  4 root  admin  128  5 Jul 12:12 configuration//

not writable by anybody but root. Why root? Because we had to install as an administrator. See part 1.

Remember to be excellent,

Andrei from The Great White North.

1 REPLY 1
Semer CHERNI
ST Employee

Hello @Andrei Chichak 

First let me thank you for posting.

I made the test with a MAC 14.5 machine and I was not able to reproduce the same behavior.

Could you start STM32CubeMX via terminal and share the content of the terminal.

BR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.