2018-09-13 01:05 AM
I migrated CubeMX 4.25 to 4.26.1 and after migrating my project I cannot access the project anymore. I have the sandbox running I can access the generation code (did not try to generate new code).
I have attached the .ioc file.
2018-09-13 05:46 AM
Please report via Online support, I can confirm issue loading it into Mx 4.26.1 (no crash, but loading is unfinished).
2018-09-13 06:58 AM
Hello,
This issue is raised internally to CubeMx team for check. We will come back to you as soon as possible.
Thank you for your contirbution.
With Regards,
Imen.
2018-09-14 05:58 AM
Hello,
I answered to your request in online support and answer here to share the information.
This issue is already known and is a regression related to ADC on 4.26.1
It should be solved on release 4.27.
By this time you can use the 4.26.0
Just edit the IOC file to set version to 4.26.0 before that to allow openning of IOC.
Best regards
Jocelyn
Update : The cube MX 4.27 is already available. You can open your project with it :smiling_face_with_smiling_eyes: