cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE - the CubeMX part suggestion

TDJ
Lead

Hi ST,

this is really not a question but suggestions.

  1. When starting a project for STM32F7x board almost 1.3 GB (!) STM32Cube_FW_F7_V1.15.0 file gets downloaded. The download often breaks, it seems like download error handling and resume is not implemented. I ended up downloading the file manually and unzipping it to user/Repository location. Otherwise it would never worked. I suggest optimizing the download process, so only files needed for the selected board/mcu are downloaded and download can be auto resumed.
  2. Some listed board names are inconsistent with product codes. For example STM32F769I-DISC0 board is listed as 32F769IDISCOVERY while its version without display is (correctly) listed as STM32F769-DISC1. Believe or not but for 20 min I was convinced my board was not supported as I could not find it. Just a bad initial experience.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Markus GIRDLAND
ST Employee

Thanks for the feedback. I'll see if I can get this to the CubeMX team, I know they're already working hard to improve this.