cancel
Showing results for 
Search instead for 
Did you mean: 

CUBEIDE Bug in RTC Generation

farukisiker
Associate II

Hello,

In CubeIDE I try to generate RTC code which has decimal parameters. However in code generation I realized that it converted to hex value by itself.

You can check screen shots in the attachment.

 

4 REPLIES 4
Souhaib MAZHOUD
ST Employee

Hello @farukisiker 

Thank you for posting!

Could you mention the name of the MCU where you encountered the issue?

KR,

Souhaib

TDK
Guru

TDK_1-1741686298843.png

This behavior is correct. 12 decimal expressed in BCD format is 0x12. If you change it to binary format, it will be 12.

If you feel a post has answered your question, please click "Accept as Solution".

Stm32H7 Series

You can check that video to ensure that there is a problem here. 

BCD only shows that the number is between 0-9. It even does not accept hex value during configuration.