cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE 1.16.0 (MX6.12.0) STM32G0B1CCU ADC1 poblem

MHoll.2
Senior

Hi,

I have tried to load a Project (.ioc file) build with CubeIDE 1.15.0 in the newly released CubeIDE1.16.0 (with CubeMX 6.12.0).

This give me an error on ADC1:

1) I can't select Vbat as ADC source (as working on CubeMX 6.11.0)

2) I get a warning about ADC_Regulare_ConversationMode

The attached picture shows to the left the 1.16.0 and to right the 1.15.0 version

ADC1_problem.jpg

Is this a known problem with the CubeMX 6.12.0?

 

1 ACCEPTED SOLUTION

Accepted Solutions

Thank you so much for reporting this issue. I confirm it on my side and I've escalated it to the Concerned team for correction (under tickets number 186012 and 186009).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
STTwo-32
ST Employee

Hello @MHoll.2 

Could you please share your .ioc file and a screenshot of the warning if possible.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi STTwo-23

Attached a sample .io file made with MX 6.11.0

If You open it with MX 6.12.0 without migration the ADC1 is OK (Vbat is present and there is no error).

If You migrate the file with MX 6.12.0 Vbat is missing and there is a error.

ADC_MX_6.12.0.jpg

Thank you so much for reporting this issue. I confirm it on my side and I've escalated it to the Concerned team for correction (under tickets number 186012 and 186009).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.