cancel
Showing results for 
Search instead for 
Did you mean: 

Cube MX and ADC4 - Channel not initialised

Markko67
Associate II

HI

I use Cube MX with STM32U585RIT6. 

When I use ADC4 In3 In4 In9 In22 and In23, the  channel In9 is not properly initialised. 

I must add this manually :

/* USER CODE BEGIN ADC4_Init 2 */
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_9;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}

/* USER CODE END ADC4_Init 2 */

With the STM32U585VIT, I have the same problem with channel9 dont work 

Then it work. I have this probleme in CubeMX from 6.9 to 6.11 versions.

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Markko67 

This issue is solved on the new release of the STM32CubeMX (V6.12.0).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @Markko67 

Thank you for reporting this issue. I can reproduce it on my side. I've report it internally to the concerned team for correction on the next releases (under internal ticket niumber 179275).

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

STTwo-32
ST Employee

Hello @Markko67 

This issue is solved on the new release of the STM32CubeMX (V6.12.0).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.