2026-01-13 4:58 AM - last edited on 2026-02-27 3:32 AM by KDJEM.1
I have a Discovery board B-L072Z-LRWAN1 and I am trying to set up a project using CubeIDE but get the following,
So I check to see if the L0 & LRWAN packages are in the repository,
Yes, they're there. I click OK & Cube carries on setting itself up & up pops the ioc window. I press configure & generate & get some C code but the build option is greyed out.
What am I missing here?
Solved! Go to Solution.
2026-01-14 5:59 AM
Thanks Mattias, I was confused about why it wasn't finding the FW in the repository as this wasn't an issue with any of the other boards we use.