2025-07-21 12:13 AM
I was creating an stm32 project for my stm32f411ceu6 dev board and when i opened the project i was not able to find the corresponding .ioc file for the board in order to configure the pins and clock for my use.
When i created the project it showed the following error:
Error downloading the following files:
mcusAds.json._tmp_(Problem during download).
2025-08-01 7:30 AM
Hello @yadukrishnan_p and welcome to the community,
Which STM32CubeIDE version are you using?
Could you please share your project?
Could you please refer to UM2609 precisely section "2.1.2 Creating a new STM32 project" and follow the steps.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.