2023-10-11 5:39 AM - edited 2023-10-11 5:40 AM
I started using the new "User Actions" feature, and it seems that there's an issue with the function that allows running a script after code generation. I managed to make the feature work without any problems when the "Window -> Outputs" option is checked. However, when it's unchecked, CubeMx completely freezes. In such cases, you have to terminate its process through the task manager, which is not desirable.
For information, I use ".bat" file. CubeMx version 6.9.2
Solved! Go to Solution.
2023-10-27 8:40 AM
Hello,
The issue is escalated to the developers and it's under investigation.
Internal ticket number: 164200 (This is an internal tracking number and is not accessible or usable by customers).
BR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-12 7:27 AM
Hello @Jdescot
Thank you for having reported the issue.
I escalated this internally to STM32CubeMx team for check and will come back to you soon with update.
Thanks
Imen
2023-10-19 10:17 AM
Hello @Jdescot
First let me thank you for posting.
Could you share the content of the script you are using. In fact at the moment CubeMX have an issue under investigation about "Pause" command in the script.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-20 4:30 AM - edited 2023-10-25 7:02 AM
cubemx_post_gen should be ".bat" file.
Example of content :
C: & cd C:\repo\simple_project & powershell -command "remref"
remref content (it's a powershell function) :
function RemoveReference([String]$repo, [String]$project)
{
$PSDefaultParameterValues = @{ '*:Encoding' = 'utf8' }
$file_name = ".cproject"
$regex_replace = "\t+<listOptionValue builtIn.+\/Users\/.+"
(Get-Content $file_name) -replace $regex_replace, '' | Set-Content $file_name
(gc $file_name) | ? { $_.trim() -ne "" } | set-content $file_name
}
New-Alias -Name remref -Value RemoveReference -Option AllScope
As you can see, there is no "Pause" related function.
Thank you,
Joël
2023-10-27 8:40 AM
Hello,
The issue is escalated to the developers and it's under investigation.
Internal ticket number: 164200 (This is an internal tracking number and is not accessible or usable by customers).
BR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-22 10:14 AM
Any update ?
2024-02-01 12:44 PM
Any updates ?
Thank you !
2024-02-02 5:09 AM
Hell @Jdescot
Sorry for the delay to respond.
The case is under investigation by our teams. I will keep you updated when the fix is implemented.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.