2024-12-01 3:40 PM
Hello STM-Team,
I'm working on my project with an STM32H723ZG and ran into an issue with the code generation when I selected "Network Interfaces" in the AZRTOS configuration.
The code generation will add "NX_ETH_INTERFACE_ENABLED" to the "RTE_Components.h" but forget the "#define" in front of it.
That is somewhat annoying because I have to manually add this everytime I regenerate the code.
2024-12-01 11:02 PM - edited 2024-12-01 11:20 PM
Hello @Intector
Thank you so much for sharing this input. I'm able to reproduce this behavior and I've escalated for correction on the coming releases (under internal ticket number 197441).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.