cancel
Showing results for 
Search instead for 
Did you mean: 

BUG CubeMX for Nucleo L4R5ZI

Posted on May 16, 2018 at 16:13

Hi CUBEMX Team,

for NucleoL4R5ZI 

LPUART1 is taking as GPIOC port. 

It has to be GPIOG port. 

0690X0000060KdkQAE.png

Please fix this 

Thanks

Phanirajkiran

#cubemx #bug
1 ACCEPTED SOLUTION

Accepted Solutions
Nawres GHARBI
ST Employee
Posted on May 21, 2018 at 11:10

Hi 

Phanirajkiran, 

When loading the board, please select init peripherals and the LPUART will be at the right port. 

Enabling manually the peripheral will select the first available port and not the dedicated one on the board

View solution in original post

4 REPLIES 4
Imen.D
ST Employee
Posted on May 16, 2018 at 16:58

Hello

phanirajkiran.ma

,

Which CubeMx version are you using?

With Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on May 16, 2018 at 17:05

Hi Imen,

0690X0000060KkvQAE.png

When  i clear pinouts and select LPUART it will go to GPIOC instead of GPIOG.

Thanks

Phanirajkiran

Posted on May 16, 2018 at 17:12

V4.24.0 is NOT current, try using the current version to confirm if the issue exists or has been fixed in the intervening months...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Nawres GHARBI
ST Employee
Posted on May 21, 2018 at 11:10

Hi 

Phanirajkiran, 

When loading the board, please select init peripherals and the LPUART will be at the right port. 

Enabling manually the peripheral will select the first available port and not the dedicated one on the board