cancel
Showing results for 
Search instead for 
Did you mean: 

B-L475-IOT01A+FREERTOS+X-CUBE-BLE1 does not build

CLiu.0
Associate

Hi there,

I am using the latest CubeMX to generate code for B-L475-IOT01A with FREERTOS and X-CUBE-BLE1 4.4.0. However the code it generate does not even build. I tried various samples, including SensorDemoBLESensor, Beacon, but yield the same result.

The build message indicated that MX_BlueNRG_MS_Init() is missing. Apparently it is missing an entire suite of source code. I attempt to port the code over from a Nucleo sample code but was unsuccessful.

Please kindly help to fix. Thanks!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Karl Yamashita
Principal

Yeah I've complained about the same issue over a year ago with support. I too can't get it to compile without so many errors. I still haven't seen ST fix the compile errors since then.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

DGarc.5
Associate II

Any answer?